FAQ Plate Multiprinter

Question:

Why does not the printer not want to insert the material for printing?

 

Answer:

You probably insert the material too fast or forgot to press online

  • Adjust the metal rails to the width of the material
  • Insert the material slowly until you hear a "bip"
  • Press online button and make sure the online lamp is on

 

 


Question:

Why don't the printer print all of the text on the material?

 

Answer:

There may be several things to check.

  • Make sure the ribbon is correctly mounted, see the instructions under the lid
  • Adjust the metal rails to the width of the label material
  • Clean the material from grease stains, dust etc.
  • Insert the label material slowly until you hear a bip
FLEXIMARK Multiprinter ribbon Multiskrivare